This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5411-Q1: Can you kindly help review the schematic diagram? Thank you!

Part Number: TAS5411-Q1


Dears,

Can you kindly help review the schematic diagram? Thank you!TI_AMP_TAS5411-Q1.pdf

  • Hello Peter,

    I have reviewed the schematic.  Here are the changes:

    1. R1322 should be equal to the parallel value of R1316 and R1319.  In this case it should be 2.35k or standard value that is close.
    2. C1053 should be equal to the parallel value of C1050 and C1052.  In this case it should be 4.4uF, but use 4.7uF
    3. There should be come capacitors between L146 and BBAT flag.  These are for EMI reduction.  Look at the schematic in the datasheet for values.

    I do not see any other changes needed.

    Regards,
    Gregg Scott