Part Number: TAS5822M
Hi TI TEAM
I would like to know that changing the 0.47uF capacitor to 2.2uF capacitor for the BST pin of TAS5822M chip will cause problems for the chip,
thanks!
Harrison
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jesse
The reason is that Ti FAE asked us to change the BST foot into 1uf capacitor at the beginning, and there would be over-current protection during our production. Later, TI FAE asked us to change the BST foot into 2.2uf capacitor, and the test result was OK。
We want to know whether the MOS tube inside the chip will be affected by changing the BST pin capacitor beyond the MOS tube Rds pin current。
Thanks!
Harrison
Hi,
many factors might affect OC.
changing to 2.2uF do help solving problem, but according to our study, 1uF-2.2uF should not have that large difference.
usually, 0.47uF should be enough.
you can confirm below several things:
1. what is your DC bias of BST cap? usually, we need it large than 7v.
2. what is your inductor Isat of LC filter, it should be larger enough than your output peak current.
3. have you connect the load when performing the test?
4. have you tried using lower switching frequency?
thanks.
Donny