Other Parts Discussed in Thread: TLV320AIC3104, TAS2781
Hi,
We are working whit a custom board based on the imx8mp that has the TLV320AIC34 codec connected to the SAI3. The OS has been generated using Yocto hardknott and the NXP BSP. We are using the kernel version 5.10.72.
We cannot configure a sound card in device-tree for the codec. Since this codec internally is composed of two tlv320aic3104, we first tried to follow an approach that consists of creating a single "simple-audio-card" node card that has two dai-links one for each codec block and using TDM. Following this approach we wanted to have a single card with four independent channels.
The device tree we have built is:
sound-codec { compatible = "simple-audio-card"; simple-audio-card,name = "ep200-audio"; status = "okay"; simple-audio-card,widgets = "Microphone", "Mic Jack", "Line", "Line Out", "Line", "Line In", "Headphone", "Headphone Jack"; simple-audio-card,routing = "MIC2L a", "Mic Jack", "MIC2L b", "Mic Jack", "MIC2L a", "Mic Jack", "MIC2L b", "Mic Jack", "Mic Jack", "Mic Bias a", "Mic Jack", "Mic Bias b", "Line Out", "LLOUT a", "Line Out", "LLOUT b", "Line Out", "RLOUT a", "Line Out", "RLOUT b", "RLOUT a", "Playback a", "RLOUT b", "Playback b", "LLOUT a", "Playback a", "LLOUT b", "Playback b", "Headphone Jack", "HPLOUT a", "Headphone Jack", "HPLOUT b", "Headphone Jack", "HPROUT a", "Headphone Jack", "HPROUT b", "LINE1L a", "Line In", "LINE1L b", "Line In", "LINE1R a", "Line In", "LINE1R b", "Line In"; simple-audio-card,dai-link@0 { format = "i2s"; bitclock-master = <&dailink_master>; frame-master = <&dailink_master>; dailink_master: cpu { sound-dai = <&sai3>; dai-tdm-slot-num = <8>; dai-tdm-slot-width = <32>; dai-tdm-slot-tx-mask = <1 1 1 1 0 0 0 0>; dai-tdm-slot-rx-mask = <1 1 1 1 0 0 0 0>; }; codec { sound-dai = <&tlv320aic3104a>; clocks = <&clk IMX8MP_CLK_SAI3>; }; }; simple-audio-card,dai-link@1 { format = "i2s"; bitclock-master = <&dailink_master2>; frame-master = <&dailink_master2>; dailink_master2: cpu { sound-dai = <&sai3>; dai-tdm-slot-num = <8>; dai-tdm-slot-width = <32>; dai-tdm-slot-tx-mask = <0 0 0 0 1 1 1 1>; dai-tdm-slot-rx-mask = <0 0 0 0 1 1 1 1>; }; codec { sound-dai = <&tlv320aic3104b>; clocks = <&clk IMX8MP_CLK_SAI3>; }; }; };
And in the i2c node:
&i2c3 { clock-frequency = <400000>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_i2c3>; status = "okay"; tlv320aic3104a: tlv320aic3104a@18 { #sound-dai-cells = <0>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_tlv320>; compatible = "ti,tlv320aic3104_a"; reg = <0x18>; status = "okay"; reset-gpios = <&gpio3 24 GPIO_ACTIVE_LOW>; }; tlv320aic3104b: tlv320aic3104b@19 { #sound-dai-cells = <0>; //pinctrl-names = "default"; //pinctrl-0 = <&pinctrl_tlv320>; compatible = "ti,tlv320aic3104_b"; reg = <0x19>; status = "okay"; //reset-gpios = <&gpio3 24 GPIO_ACTIVE_LOW>; }; };
We have had to create a new tlv320aic3104 driver where we have added the sufix "_a" and "_b" in order to avoid to have controls with the same name.
When the system is booted, we can see one card (ep200audio) with two devices:
card 1: ep200audio [ep200-audio], device 0: 30c30000.sai-tlv320aic3x-hifi tlv3 20aic3x-hifi-0 [30c30000.sai-tlv320aic3x-hifi tlv320aic3x-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 1: ep200audio [ep200-audio], device 1: 30c30000.sai-tlv320aic3x-b-hifi tl v320aic3x-b-hifi-1 [30c30000.sai-tlv320aic3x-b-hifi tlv320aic3x-b-hifi-1]
Subdevices: 1/1
Subdevice #0: subdevice #0
The card has the controls duplicated that allow us to control each codec block independently, by example "PCM Playback Volume a" and "PCM Playback Volume b". The problem we have is when we try to play two sounds at the same time using the two card devices, if we run the following commands in two separated consoles, no sound is played and the commands don't finish:
aplay /usr/share/sounds/alsa/Front_Center.wav -Dplughw:ep200audio,0
aplay /usr/share/sounds/alsa/Front_Center.wav -Dplughw:ep200audio,1
Is our approach correct? How can we solve this problem? In our application we need to play sound in the two devices at the same time.
Regards,
Gustavo Plaza.