Hello,
I execute the following commands.
//======PHONES OUT ========// //Table 53. Page 0/Register 47: DAC_L1 to HPLOUT Volume Control Register writeRegister(wires, dev, Page_00, 47, 0x80); //Table 70. Page 0/Register 64: DAC_R1 to HPROUT Volume Control Register writeRegister(wires, dev, Page_00, 64, 0x80); // Table 57. Page 0/Register 51: HPLOUT Output Level Control Register writeRegister(wires, dev, Page_00, 51, 0b10011101); // Table 71. Page 0/Register 65: HPROUT Output Level Control Register writeRegister(wires, dev, Page_00, 65, 0b10011101); //===========RCA OUT===============// //Table 60. Page 0/Register 54: DAC_L1 to HPLCOM Volume Control Register writeRegister(wires, dev, Page_00, 54, 0b10000000); // Table 77. Page 0/Register 71: DAC_R1 to HPRCOM Volume Control Register writeRegister(wires, dev, Page_00, 71, 0b10000000); //Table 64. Page 0/Register 58: HPLCOM Output Level Control Register writeRegister(wire1, 0x18, Page_00, 58, 0b10011101); //Table 78. Page 0/Register 72: HPRCOM Output Level Control Register writeRegister(wire1, 0x18, Page_00, 72, 0b10011101);
But for some reason I'm getting LEFT only on HPLOUT/HPROUT and RIGHT only on HPLCOM/HPRCOM. Is there something that you can imagine that I'm doing wrong?
I know that I'm getting stereo separation on the DAC>DACVolume register because I can confirm left on left and right on right. Just not LEFT/RIGHT for each pair...
Does anyone have some things I can look into? Thank you!
Jay