Other Parts Discussed in Thread: BQ25120A
Hello, I'm using the bq25120A on a printed board and when the battery is reaching a certain level of discharge, around 3.3 V and under, I have I2C communication problem, and the BQ become default value 1.8 V instead of what I put in the register (3.0V or 3.V). Could you help please, what could I change in the register?