Other Parts Discussed in Thread: TLV320AIC3111
Hello, we have TLV320AIC3111 EVM board and working out the best speaker and microphone can be used on the eval board as external components and test the AGC feature of the codec.
From datasheet:
- Headphones must be 16 Ohms 60mW or 32 Ohms with 20mW.
- Speaker to be Stereo 8 Ohms differential around 790mW to 1.29W (basically 400mW per channel)
- What would be for microphone?
Are these details enough to filter the speakers and headphones?
Thanks