Other Parts Discussed in Thread: PCM1792A, PGA2310, PGA2320
Hello,
Please help me to get this right: I have to decide whether to use the PCM1792A's integrated volume control / attenuator or to use the 1792 together with a PGA2310/2320 volume control. Goal is the highest possible sound quality, even with low volume levels (attenuation, say -40dB). The circuit will feed right into a power amplifier.
As the PCM1792A's volume control works in the digital domain, I'm not sure if it will affect or even degrade THD performance. If I set the attenuator to -40dB for example, the wanted signal will be attenuated this amout. But the distortions won't be attenuated, as they originate in the DAC stage (right?). Therefore, the output signal's THD performance degrades from the specified -108dB (0,0004% @Fs 44,1kHz) to -68dB.
Opposed to that, when using a external attenuator like the PGA2320 set to -40dB, it will attenuate not only the wanted signal, but also the distortions, so the THD performance will stay unaffected. Of course, the PGA2320's own THD will dominate in this configuration. Unfortunately, it is only specified at 0dB Gain (with -108dB), there is no data for THD vs. Gain or THD vs. output amplitude. But I expect THD to decrease with higher attenuation.
So the PGA2320 solution will be far superior to the PCM1792A's integrated attenuator, won't it? Am I missing something here?
Thank you very much for any suggestions.
finalstage