Part Number: TLV320DAC3100
what is the max operating current consumption of AVDD, DVDD,HPVDD,SPKVDD and IOVDD respective rails for TLV320DAC3100.
under 1W ,2W output across 8ohm speaker and max HP gain
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV320DAC3100
what is the max operating current consumption of AVDD, DVDD,HPVDD,SPKVDD and IOVDD respective rails for TLV320DAC3100.
under 1W ,2W output across 8ohm speaker and max HP gain
Hi Bhavesh,
I can plan to test this over next week, however this will be a test on a single device and there may be some variation from one device to another.
You mentioned max HP gain but 1W, 2W on 8ohm, do you mean you'll have both amps (SPKR and HP) at the same time?
Best regards,
-Ivan Salazar
Applications Engineer
Hi Ivan,
I am ok with the variation since I need figures to calculate my system power consumption.
Your correct SPK and HP would not be at same time.
Regards
Bhavesh
Hi Bhavesh,
Understood, I'll come back with further test plan soon.
Best regards,
-Ivan Salazar
Applications Engineer
Hi Bhavesh,
I took some current measurements for 1W case:
| 1W | |
|---|---|
| AVDD | 2.51mA |
| SPVDD | 268mA |
| HPVDD | 5.05mA |
| IOVDD | 0.021mA |
| DVDD | 3.92mA |
| Total | 279.501mA |
The EVM is powered from USB-5V. I didn't capture 2W as that is actually too high THD+N levels (>15%) as you can see on data sheet figures 4-11 and 4-12.
If you have an EVM you can also run measurements for any other configuration.
Best regards,
-Ivan Salazar
Applications Engineer