Part Number: TPA2011D1YFFEVM
Hello,
I am evaluating the TPA2011 using the EVM module and I have a question:
I am passing it though a LPF with a cutoff at 60 kHz so to remove the 300 kHz switching modulation. Then I am driving a resistive load.
This works pretty well when using a sine waveform. Triangular waveforms works as well.
I am most interested in a square waveform. When the amplitude is <0.9V it works well, but when the amplitude is greater than 0.9 V it will execute just a few periods and then the output switches to zero.
I imagine there is some kind of feedback that actively suppresses the square-wave. is this true? Is there a way around it?
Are there other eval kits that are better suited?
Kind regards,
Matthias