This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3120: Headset Detection Functionality clarification

Part Number: TLV320AIC3120


Hi,

We are using TLV320AIC3120 codec in our board. I have a doubts regarding Headset detection/ mic det functionality. 

In datasheet, it is mentioned that I have to configure Page 0 register 67(0x43). Consider I'm using standard headset jack which is connected with mic and speaker.

So, the doubt is 

  1. For bit D4-D2, how will I get to know what is the debouncing time and Is there any standard timing that I can write?
  2. Consider I'm not going to use button press detection . In that case Do I have write 00(0 ms) for for bit D1–D0?