This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM4202 - system clock and bit clock

Other Parts Discussed in Thread: PCM4202, TAS5518C, TMS320C6720

In datasheet on PCM4202 I see what system clock on 192kHz mode (quad mode) can be 128 or 192 Fs. I want to use PCM4202 in PCM slave mode. What frequency bit clock I must or can supply to ADC from Master? My system consist of TMS320C6720 works as master and transmit 2 data signals to TAS5518C. DAC must add one data signal to TAS5518C in the same clocks as DSP. TAS5518C utilize only 64x bit clock. Will PCM4202 works parallel to DSP on 64x bit clock?