Part Number: SRC4382
Other Parts Discussed in Thread: DIX4192, SRC4392, , SRC4190
Hello,
Do we have a p2p alternative to the CS8422 from Cirrus Logic? It is EOL.
Best regards,
Ambroise
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ambroise,
CS8422 is 32 pin device and SRC4382 is a 48 pin device so it is not pin to pin compatible ( SRC4382 is also compatible with the SRC4392 and DIX4192.)
The other option is SRC4190 or SRC4192 which are 28 pin and operated from a Single 3.3-V Power Supply. Either way they need to do some board modification.
Let me know if I can be of any help.
Regards,
Arash