Other Parts Discussed in Thread: TAS5751M
Hello, I use the TAS5751M chip in accordance with the EVM board amplifier, distortion and signal-to-noise ratio is normal, but only the frequency response attenuation is too large, the first chart below is my load 8 ohms, input signal 1kHz sine wave and 0dBu when the AP repeatedly measured the amplifier frequency response graph, the low frequency part of the graph attenuation 3.5dB, high frequency part of the attenuation of 4 to 8dB very unstable And we want to achieve the attenuation in about 1dB. The second picture and the third picture are the schematic diagram and PCB of my amplifier part.
I would like to ask the following questions.
1, do you have the chip frequency response curve, I want to know the normal frequency response of the chip, whether it can reach the 1dB attenuation requirements, I did not find in the specifications.
2, the amplifier analog output of the LC filter device selection and the official EVM board model and size is the same, but the frequency response is very poor, is it related to the internal configuration of the chip, how do I need to configure?