Part Number: LM4675SDBD
Other Parts Discussed in Thread: TPA2015D1, LM4675
Hi TI Team,
We are using the LM4675SD/NOPB in one of our designs, and the audio output of the speaker is not satisfactory.
We used speaker with 8R, 0.7W input power (1W Maxe), and 94 dBA SPL specifications.
We have given the Lipo battery voltage (3.7 V, 450 mAh) as the supply voltage of the LM4675SD. As per the datasheet, in Figure 5 (Output Power Vs. THD), It looks like at 3.7V, the LM4675SD can give 0.5–0.6W as output. Can you please confirm the same?
I have a physical sample, and I want to measure the peak output power of the LM4675SD using CRO. Can you please suggest a method and filter value between LM4675SD output and CRO?
As far as I know, we can input a fixed sine wave to the amplifier, and we need to use a filter between the amplifier output and the CRO. We need to measure the maximum amplitude of the output signal without clipping, and by P=E^2/R we can calculate the output power of the amplifier.