This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM6240-Q1: How to create the firmware bin for PCM6240

Part Number: PCM6240-Q1
Other Parts Discussed in Thread: TAS2558

Hello, TI engineer:

Please help answer the following 2 questions, thank you!

  1. The current project uses the PCM6240 ADC, and only the PCM6260 driver can be found on the TI official website. Can the PCM6240 use the PCM6260 driver? If it can be used, what are the differences that need to be modified?

  2. When downloading the pcmdevice-linux-driver from the main branch of the driver code, the tool utility opens with a device list consisting of tas2558 and other PA devices. In the use of the PCM6260 driver, we need to generate a bin file for the configuration of the registers. How can we generate a pcm6240.bin file?

BR,

wen gu