Part Number: PCM1840
Other Parts Discussed in Thread: PCM1804, , PCM1821, PCM5102A, TLV320DAC3203
Hello,
Our customer validate PCM1804 function at slave mode 32BCK I2S input from BT module with internal PLL mode which reference to BCK input.
In this BT module outputted 32BCK clock is unique, 37nsec shorter clock is popped up around every 1sec. It seems BT module to adjust long time average of sampling frequency to 48KHz 32BCK rate from 24.0MHz master clock.
Resulted in PCM1840 PLL could not lock with this BCK reference input, we could not see SDOUT signal, keep the pin high-z.
Is there any workaround to support this strange BCK clock input.
We plan to evaluate PCM1821 PLL mode instead, but is there same PLL IP block used from PCM1840 and will it give us same result?
Regards,
Mochizuki