Hi team
Customer use TPA6304-Q1 in ford project, but cannot pass the EMC test use the suggest design, here are some questions:
1. What will cause the EMC issue in 20MHz 60MHz 100MHz 200MHz when there is no overshoot and ring in the output stage? How can I solve that?
2. When customer test the EMC in Iveco, after the amp power on they can test a 200kHz radiation, will the amp can generate the 200kHz radiation directly or it may cause by the DCDC power supply?
here is the EMC test waveform:

after add the magnetic beads in the output stage, the EMC problem can be solved, but it can cause over current issue in some time.

when I test the output stage of 6304 the waveform is good without any overshoot and ring.

Thank you
Best Regards
Joe
JUL 27