Part Number: SRC4190
Hello Experts,
My customer would like to use RCKI=49MHz in input/output are slave mode. Is there any concern? The sampling rate will be 192KHz.
Best Regards,
Fujiwara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SRC4190
Hello Experts,
My customer would like to use RCKI=49MHz in input/output are slave mode. Is there any concern? The sampling rate will be 192KHz.
Best Regards,
Fujiwara
Hi Fujiwara;
Max RCKI is 50MHz, so 49MHz should be okay. refer to Figure 64. Reference Clock Input Connections and Timing Requirements to stay within RCKI requirement.
Use Table 1. (Setting the Serial Port Modes) to set the input and output in slave mode.
Regards,
Arash