Part Number: TPA3116D2
Hi,
I have a serious problem of audio cutting out (not wave chopping , o/p turns off completely) every few minutes or sometimes seconds and the resumes . I have the o/p connected to a 100V LMT (Line matching Transformer) as the speakers used in the application have an LMT too and need a 0-100V audio i/p.
The circuit used is shown - very similar to the one in the datasheet. I have had to bypass the o/p filter as well as using heats up the device significantly.
The problem seems similar to the one reported on the diyaudio link below but it only happens at high volume (not low volume as reported in the link below. The effect is similar to that seen here -https://www.youtube.com/watch?v=fCSD2zig2lw
Any help on this problem will be appreciated.