Part Number: TAS5825M
Using the purepath standard 2.1 model and referencing the DRC tweeter
When I change fc1 the low pass frequency from 1000 to 500 hz
( which appears to update both fc1and fc2 together
I get he following I2c capture
w 98 00 10
w 98 60 00 02 18 76 00 04 30 ec 00 02 18 76 0f 42 90 36 f8 b5 0d f2
w 98 74 00 08 05 2e 00 10 0a 5b 00 08 05 2e
w 98 00 11
w 98 08 0e 85 d1 8c f9 5a 19 be
It appears that the update command sequence for the second filter requires a rolls over from page 10 to page 11.
My questions is this rollover expliitly require to change the page or will writing to 74 rollover automatically