Audio Amplifier details is below which we are using in current model
|
VPN |
MPN |
|
P701127DFA0000 |
TAS5720ATDAPRQ1 |
This amplifier can support up to 25 W, but we were using 0.5 W rated power speaker. Speaker is failing when we are operating @ 2 KHz ( Measured Image is attached in output side )
Is there any possibilities to reduce the Gain by Software via I2C by changing the register settings.
SPK_GAIN0 (11) & SPK_GAIN1 (12) both are pulled up with 3.3 V. It is configured as Software control.
But Datasheet, Page No 30 , A_GAIN = 00 ( In description If 11: This setting is reserved and must not be used). So whether we can able to use or not.
We have seen in datasheet Right & Left volume control, May I know what is the relationship between Gain & Volume. If we are going to reducing the volume of the speaker, we can safeguard speaker by using the same amplifier.
Please share comments at earliest. Thanks in advance.
Note : DVP is completed, we can’t able to change PWB level