Part Number: PCM6260-Q1
Hello,
About PCM6260 input attenuator, I'd like to confirm the DC-Coupled Microphone Differential Input mode is -14dB, what about DC-Coupled Microphone single-ended l Input mode,-8dB?
Differential mode: -14dB=20log(2.828/14.14),
single-ended mode: -8dB=20log(2.828/7.07)
Our customer's application is as following:
Theoretical calculation: We want no attenuation on the path, considering MIC has intrinsic μV - 10.5dB attenuation, ADC intrinsic μV - 8dB attenuation, so the gain is set to GAIN =8dB, Volume10.5dB actually tested: we used ALSA tinycap recording to get PCM files, The sample value was read through the Au software and a mismatch was found with the theoretical value. If the theoretically calculated ADC intrinsic μC- 8dB is changed to 0dB, it will match the actual test.
In addition, here is the ADC registers configuration, please help to check if they are proper.
Best regards
kailyn