This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5825M: Time order of TAS5825 apply in customer system

Part Number: TAS5825M
Other Parts Discussed in Thread: TAS5805

Hi team

TAS5825 is used in array microphone system by customer, the amplifier is used to playback the voice which collected by an ADC.

In the system design, there is no data buffer for ADC, so TAS5825 must ready before ADC transmit the data to it, otherwise, the system might stuck.

Since the initialization process of TAS5825 should take a long time (around 5s) every time when the audio start to play, the system time order cannot be fulfilled.

The question is:

1. Can TAS5825 keep the configuration in DSP once the device powered up, but not reconfigured every time when the audio need to be played.

2. Do we have the startup configuration demo in Linux system to demo for customer?

Thank you!

Best regards

Joe

AUG 21