Part Number: PCM2912A
Other Parts Discussed in Thread: TPA3137D2
Hi Ti team,
Our audio signalchain is : x86 CPU ---(HDA)---> codec ALC892 --(two line out)-> TPA3137 --> two stereo L/R differential outputs audio..
http://chipset-ic.com/datasheet/ALC892.pdf
now we hope to change to USB interfaced codec like PCM2912A. I am not familiar with audio things, some questions to consult:
1. ALC892 support 44.1K/48K/96K/192K sample rate, while PCM2912A max support 48 kHz. Not sure whether this will be enough. we use 44.1K now, but may upgrade to higher sample rate.
2. ALC892 support 16/20/24bit , while while PCM2912A support 16bit DAC. Not sure whether this resolution will be enough.
3. PCM2912A only have one stereo output, so I need to use two PCM2912A ? or other solutions?
4. any other suggestions are welcome.
Thanks!