Im connecting OPA1637DGK differential outputs to a PCM1865, Im having toruble understanding the common-mode voltage connection. Do I need it? When do I need it? I thought i did so i connected them as shown in the pitcture, but im not sure i need this connection. Just to clarify they are in separate boards connected through a connector, these are the pictures of the schematic. I might not need to connect VCOM because i dont see any common voltage requirements on the PCM, but i still cant wrap my head around it