Part Number: TPA3255
Hi Dear,
The customer is looking at TPA3255 and has the following questions:
1. In the manual, for each BTL, 8 ohms per channel can achieve 155W, but the first page of the manual mentions a total power of 150W. As the following two images?How to understand this?

2. How to connect signals to the four input channels INA/B/C/D when using BTL mode to drive two speakers? Do we all need to connect signals?