Hi everyone
This is our test-setup:
- TLV320AIC3263EVM-U
- Audio coming from PC through USB
- 0dBFS
- Class D amp
- 8Ω 0.5W or 3W speakers to SPKP/SPKM
- Output filter (JP1 & JP2) enabled
- Power by USB/board or external(J16)
- Class-D playback example configuration
When testing the "Class-D playback" example configuration on CodecControl, we see that anytime we silence the incoming audio, the short-circuit self-protection kicks in, and we can only reset it by reloading the configuration or by power cycling the board, turning on/off the speaker Amp does not reset the protection.
We have seen this happen with the amp powered by either board/USB or external power(J16), 0.5W or 3W speaker.
Is there any relationship between the short-circuit protection and the audio?