Dear Sir,
I have a sound bar system that has (I2S-IN) header. The signals present on these headers are (LRCLK, BCLK, MCLK, and Data0-Data3). Of course HDMI eARC host(TV) side connector(19 pins) is sending audio signals to reciever side. I want to connect the HDMI eARC Reciever connector to our design schematics
This is the input header of my soundbar system and I want to connect the HDMI eARC connector to this header. can you plz help me in this regard?
Thanks
Ammar