Part Number: OPA2132
Other Parts Discussed in Thread: OPA2156, OPA1656
Hello
Can you give me an equivalent to the AOP OPA2132U that we are unable to supply, on the site you recommend OPA2156ID which is a CMOS amplifier.
Thank you for your help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
For a JFET input device (meaning very low input bias current and also very low 1/f noise), you can try OPA1642 - it is very similar to OPA2132 and also comes in the SOIC package.
For lower wideband noise and overall more bandwidth, the OPA1656 is also a good choice. It is not a JFET input, but a MOSFET input. This means the 1/f noise is not quite as low but the wideband noise and overall distortion is better. This is similar to OPA2156 but optimized for audio.
Let us know if either of these can work.
Best Regards,
Mike
Hello,
The OPA2132U give a max input offset voltage of 0.5mV and the OPA1656 3.5mV.
That's the only thing that bothers me when I compare the 2 refs.
Best Regards
Hi,
OK yes I was thinking of the lower grade OPA2132, which has Vos of 2 mV. But for lower offset, then indeed the OPA2156 is a good choice. For JFET input devices, the OPA2140 is the best cross.
Best Regards,
Mike