The inductors and ic on the mono subwoofer channel (PBTL) om my dual amplifier board are very hot. The stereo high end amp is much better and only gets warm. I measured the idle power and it’s 10W. (19,5v 0,5A) . The stereo amp is only using 1W. I’m using the Bourns SRR1280-100M. (10uH 19,5mΩ 6A Imax 6,3 Isat). I’ve tried putting a different inductor (Wurth WE-SD 744711005) with no difference. Should a inductor with a very high (<20A) Isat and Imax solve the problem?