This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5411-Q1: Short-to-GND Issue

Part Number: TAS5411-Q1


Hello team,

My customer is using TAS5411EVM board to drive the 4Ohm speaker, but the tool report the short-to-GND fault. The detail is as below:

Supply of EVM board, 12.6V

Speaker is 4Ω,they measured as 4.1Ω.

Please check the connection as below:

1. The speaker is connected to the EVM out

2. They short the out of the EVM board

Support need:

1. Please help review the test condition, and analysis why the fault is reported?

2. I see the short event is reported when the Resistance is in 0.9Ohm--1.5Ohm range, please help clarify the mechanism of how TAS5411 detect the resistance and diagnose the short-to-GND fault?

Let me know if you have any waveforms need to get from the customer 

Best regards,

Lanxi