Hello,
I built up a LM3886 with single supply voltage as described in the datasheet application (Figure 3. Typical Single Supply Audio Amplifier Application Circuit).
I added a potentiometer below "Ra" to regulate the bias voltage of the input signal.
My intention is to make a bridge amplifier and adjust the offset of both chips with that potentiometer so it becomes nearly 0V.
The problem : the Chips are oscillating at a high frequency (see picture below) as soon as I turn off the mute by bridging it to ground with "S1".
My mute circuit is CM= 68µF in parallel with RM=15k. So by closing the mute switch it should turn on the amp (or in other words turn off the mute) if I got it right.
When i do so there's an oscillation on the output with a remarkable amplitude (as shown in the picture below), on both outputs the same...
I tried desoldering one chip and just having the behaviour of one isolated, absolutely the same. I tried varying by adding or deleting some filters (stability, zobel, etc. ) as mentioned in the datasheet, with no success.