This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5825PEVM-AMPS097: Modulated Ultrasound (40 kHz) with Samplerate of 96kHz possible?

Part Number: DRV5825PEVM-AMPS097
Other Parts Discussed in Thread: DRV5825P

Hi there,

The goal of our project is to build an amplifier for a parametric speaker (ultrasonic transducer array).
Wherefore, we need to amplitude-modulate the carrier frequency of 40kHz with the audio signal (base-band).
The required bandwidth is ±5 kHz (35 kHz ... 45 kHz), which theoretically fits into the Nyquist-band of fs/2 (at 96 kHz sample rate -> BW = 48kHz).

The DRV5825P seems so be ideal for this task, as it is specially designed for capacitive piezo-electric transducers and has a loop-bandwidth (output bandwidth?) of up to 175 kHz @ Fsw 768 kHz (switching frequency).
So in theory it should be able to reproduce a output frequency of 40 kHz.

However, while testing the evaluation board, we've never were able to produce higher frequencies above ~25 kHz.
We confirmed that the input sample rate is set to 96 kHz (LRCLK measured) and the chip correctly detects it (FS_MON Register 37h -> FS = 4'b1011).

In the Pure Path Console 3 Tool, the internal sampling rate can only be set to 48 kHz (which of course is too low).
Therefore we adjusted the registers directly by setting the DSP_CTRL Register 46h -> USER_DEFINED_PROCESSING_RATE = 2'b00 (same as input, no sample rate conversation).
This didn't really help to solve the issues.

My hypothesis is that even when the pre- and post EQs are disabled, there are still some filters (interpolation?) build into the internal signal chain that have a low-pass characteristic.
My question is therefore: Is it possible to use this chipset for our application? If yes, how do i need to configure it to get the full bandwidth of up to 48 kHz (@ 96 kHz sample rate)?

I hope the information I've provided is sufficient to answer my questions.
Thanks in advance for the support!

Florian

  • Hi Florian

       I'm sorry that DRV5825P indeed can't support ultrasound using. The internal DSP resource is quite limited, can only work well under 48KHz. Even you send in 96KHz audio signal,  internally would transfer it into 48KHz to let DSP working.