This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3100: ACEV-1A EVM export command list

Part Number: TLV320AIC3100

When working with the ACEV-1A EVM GUI, it is possible to record and save (export) the command list but is it also possible to export the I2C register commands or do they have to be hand copied to the host firmware editor?

  • Hi Bruce,

    If you open the command window and check the record button, the I2C commands associated with your actions in the GUI will be displayed in the command buffer. You can then click "save" to save the instructions recorded in the buffer to a text file to be used later or by something else.

    Best regards,
    Jeff McPherson