Hi
AHD Camera video accesses DV660 MB via VX1. As described in the block diagram below. The DV607 and DV660 in blue boxes are projects that we have mass-produced. The customer plans to connect the AHD Camera's Audio to the DV660 MB The ADC and MCU in the pink box are the parts we want to implement next.

There are two types of AHD cameras, namely STSC272 and STSC201. The circuits corresponding to the Audio part are as follows The measured waveform is as shown in the attachment
Is it OK to implement ADC convert to I2S using PCM1821? Thanks
STSC272 Dome Camera Audio Circuit Schematic Diagram

STSC202 Backup Camera Audio Circuit Schematic Diagram