This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM6260-Q1: For MIC+ line shorted to battery fault; any potential risk on V_MICBIAS?

Part Number: PCM6260-Q1


Hi team,

My customer wants to know if there's any potential risk when the MIC+ input line is shorted to the battery (12V), higher than the specified V_MICBIAS = 9V. The customer is currently using the DC-Coupled Microphone Differential Input Connection. The MIC+ input line is pulled up to MICBIAS and the impedance is at 340Ohm; line impedance between MIC+ line and the INxP pin is 2.2k.

The customer is worried that the reverse current into the MICBIAS via the 340Ohm might burn the chip. Although the calculated current is only around 8.82mA (3V/340Ohm), I'm concerned that it might still do some damage, since MICBIAS is generated by a built-in boost converter and it will flow back into the 3.3V BSTVDD input via the reverse parallel diode of the high side switch and the inductor.

Could you please comment on the customer's doubts?

Thanks in advance!

Mingrui