This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC6140: No AREG, no I2S DATA

Part Number: TLV320ADC6140


Hello TI team,

I'm working with TLV320ADC6140 with 2 single ended electret mic lines. 

ADC is used in slave 1/2 channel 48kHz 32bit 

Im not getting any data on the scope. I noticed that the AREG and MICBias has no voltage.  

DREG is at 1.45v, Supplying 3.3V to analog and 1.8V to digital IO 

IRQ pin is high but I believe I disabled that.  I do measure 48.035KHz on analyzer. Would that put create bus error?

 

 

sl_sleeptimer_delay_millisecond(5);
  ADC_Write(I2C0,0x01,0b00000001); // Reset registers
  sl_sleeptimer_delay_millisecond(10);
  ADC_Write(I2C0,0x02,0b10001001); // Sleep Reg - Internal 1.8V Areg, 10ms, not sleep
  sl_sleeptimer_delay_millisecond(10);
  ADC_Write(I2C0,0x07,0b01110000); // ASI I2S 32bit Auto CLK
  sl_sleeptimer_delay_millisecond(10);
  ADC_Write(I2C0,0x08,0b00000000); //
  ADC_Write(I2C0,0x09,0b00100000); // 1 Disable Error detection

  ADC_Write(I2C0,0xA, 0b00010000); // Mixing No mix, -6dB, No inversion
  ADC_Write(I2C0,0xB, 0b00000000); // Slot 0 ch1
  ADC_Write(I2C0,0xC, 0b00000000); // Slot 0 ch2
  ADC_Write(I2C0,0xD, 0b00000000); // Slot 0 ch3

  ADC_Write(I2C0,0x13,0b00000111); // Slave automatic PLL
  //ADC_Write(I2C0,0x14,0b10001000); // not used in slave mode
  //ADC_Write(I2C0,0x15,0b10000010); // Read Only but 44.1-48 1:32 ratio BLCK FSYNC
  //ADC_Write(I2C0,0x16,0b00001000); // CLK_SRC when in Master

  ADC_Write(I2C0,0x21,0b00100101); // GPIO setup Interrupt
  ADC_Write(I2C0,0x22,0b00000001); // IN2M_GPO1 disabled act low
 // ADC_Write(I2C0,0x29,0b10000000); // Interrupt GPIO1 as GPO
  ADC_Write(I2C0,0x2B,0b00000000); //

  ADC_Write(I2C0,0x32,0b00000000); // INT ACtive high
  ADC_Write(I2C0,0x33,0b00000000); // Masking interrupt
  ADC_Write(I2C0,0x36,0b11100000); // Interupt config ASI PLL MIX Int
  ADC_Write(I2C0,0x3A,0b01100000); // Common Mode avdd peak
  ADC_Write(I2C0,0x3B,0b00000001); // IN2M Bias 2.5v
  //ch1
  ADC_Write(I2C0,0x3C,0b00100000); // CH1 setup Mic Single AC 2.5k DREoff
  ADC_Write(I2C0,0x3D,100); // CH1 Gain
  ADC_Write(I2C0,0x3E,100); // CH1 volume
  ADC_Write(I2C0,0x3F,0b10000000); // CH1 gain calibration
  //ch2
  ADC_Write(I2C0,0x41,0b00100000); // CH2 setup Mic Single DC 2.5k DREoff
  ADC_Write(I2C0,0x42,100); // CH2 Gain
  ADC_Write(I2C0,0x43,100); // CH2 volume
  ADC_Write(I2C0,0x44,0b00010000); // CH2 gain calibration

  ADC_Write(I2C0,0x6B,0b00100001); // DSP DRE HPF
  ADC_Write(I2C0,0x6C,0b00000000); // DSP clipping, volume control,
  //ADC_Write(I2C0,0x6D,0b00100000); // DRE config Dynamic Range Enhance
  //ADC_Write(I2C0,0x70,0b00100000); // AGC config Automatic Gain Control

  ADC_Write(I2C0,0x73,0b01000000); // Channel enabling input, EN1 En2

  ADC_Write(I2C0,0x74,0b01000000); // Channel enabling output, En1 En2

  ADC_Write(I2C0,0x75,0b11110000); // Power controls
  //ADC_Write(I2C0,0x76,0b11000000); // ADC power up
  //ADC_Write(I2C0,0x77,0b11100000); // Active mode

  • Hi Rafal,

    Before analyzing your script, lets ensure HW is correct, correct clocks, and power is provided to device. Can you provide comments on the following points:

    • For single-ended configuration, please implement one of the following circuit connections at input:

    • We also recommend pulling up SDA/SCL to IOVDD in I2C, but if writes to device are successful i supposed okay for now.
    • For your clocks, your confirming 48Khz status on FSYNC? What is the BCLK frequency?
    • MICBIAS is dc coupled to GND in your schematic so there will be no voltage?

    Regards,

  • Hi Dave,

    Sorry for bad schematic. Inputs are AC coupled and I2C is lifted to 1.8V. 

    BCLK hovers between 2.91MHz-3.333MHz, FSYNC 47.985KHz- 48.031KHz, analyzer shows errors. 

    I though I could measure 2.5V on MicBias pin that's going to the mics. 

    Thank you

  • Hi Rafal,

    I believe there is an ASI bus clock error. Device is in slave mode, 32-bit wordlength, the BCLK should = (32-bit WL, 2Ch, 48KHz Fs) 3.072Mhz stable, 6.144Mhz-4Ch, Frame clock input should also be a stable 48KHz.

    Please provide stable clocks and this preset configuration below:

    # CHECKSUM 0
    # Generated by ADCx140EVM-SW v3.0.5
    # TLV320ADC5140 device configuration
    # -----------------------------------------------------------------------------
    # Reset
    # -----------------------------------------------------------------------------
    # Select Page 0
    w 98 00 00
    # Reset Device
    w 98 01 01
    # 1mS Delay
    # -----------------------------------------------------------------------------
    # Begin Device Memory
    # -----------------------------------------------------------------------------
    # Page 0 (0x00) Dump
    # Select Page 0
    w 98 00 00
    # Wake up and enable AREG
    w 98 02 81
    # Clock Error Disable/Enable
    w 98 04 40
    # GPI Configuration
    w 98 3b 60
    # Channel 1 configuration
    w 98 3c a0
    # Channel 2 configuration
    w 98 41 a0
    # Channel 3 configuration
    w 98 46 a0
    # Channel 4 configuration
    w 98 4b a0
    # Channel Input/Output Configuration
    w 98 74 f0
    w 98 1e 82
    # M divider Enabled with Divider Value
    w 98 1f c0
    
    
    
    
     

    Also make sure schematic follows structure of typical application in 9.2.1 of d/s.

    Regards,