This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Support Team
we could use PCM6020-Q1 (ADC) to analysis speaker output signal, have any concern?
function block as below chart:
if any suggestion,Please advise me.
Thanks,
Best regards,
Lawrence
We need get ADC feedback data then compare original data confirm the data whether or not change by SOC
Whether or not have some different with normal design of input portion.What portion need been highlight before design
Can you please send me the maximum signal level and minimum signal frerquency coming from the DAC?
DAC Max signal level is 15W (about voltage is 7.75V),min signal frequency is 20HZ
Yes,this is base on speaker spec estimated but it’s not final result due to current speaker vendor no fix
The signal of 7.75Vpp will couple through the capacitor and shall ride on the MicBias Level. 7.75vPP implies a Vp of 3.875V..Therefor a micBias of Greater then 4V can be used.Please set 5V.
Use Ro=4k7 and C>1/2*3.14*20*4700 =1.6uf can be used. I suggest to use C=4.7U
Hypothesis the worst case Vpp is 24V (12V power level ).the MicBias level set 15V,RC follow the format it’s ok? the speaker vendor no fix,maybe spec will been change.
The maximum pin voltage is 18v . If the MicBias is coming from an outside source is 15v then i would suggest placing a series resistor in series with the coupling capacitor.. This shall form a voltage divider with the 4K7.
24*4K7/(R+4K7)=6.v
R is approx 15k
This would limit the pin voltage to 6vpp so that the pin goes to 15+(6/2) or 18v