This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6133A2: BTL Mode

Part Number: TPA6133A2
Other Parts Discussed in Thread: TPA6130A2,

Hi,

My understanding is that the TPA6130A2 has a similar architecture to the TPA6133A2 but allows the amplifier to work in a BTL configuration via I2C control.

I was wondering if the TPA6133A2 can also be used in the BTL configuration to save the need for the I2C communication. Is BTL mode tying RIGHINP and LEFTINM together internally and RIGHTINM to LEFTINP? If so could connecting these together externally allow for the TPA6133A2 to work in BTL mode?

I intend to use two TPA6133A2's in BTL mode to drive two headphone drivers in a set where higher power output is required. They will be connected to the differential outputs from a QCC5181 module.

Many Thanks,

Jonny

JCR Acoustics