This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADCx140

hello, 

       I couldn't find the information about the input resistors connection of input impedance section (2.5K, 10K or 20K) in the TLV320ADCx140 block diagram, the details as below:

1. is the resistors (2.5K, 10K or 20K) directly connected between the ADC analog input pins to Ground, or connect to a DC dias voltage (VREF/2), because we will plan to use a DC-coupling input for analog signal to ADC, and try to use internally resistors for voltage divide to make sure no clipping, thanks.