This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6584-Q1: TAS6584-Q1

Part Number: TAS6584-Q1


Dose it(TAS6584) support Output=150W*4CH@  2ohm load when it is in BTL mode、 

(1)if YES, please confirm the condiction:Voltage、Register、Output Filter

(2) if NO,it Must be in PBTL MODE?

(3)   Is there any other IC that can support Output=150W*4CH@  2ohm load when it is in BTL mode?

Thank U