We have a BT speaker product in development. It uses an Actions ATS2835P as BT SoC and system processor, which configures the TAS with I2C and streams I2S from BT source. We have a 2.0 BTL configuration.
We are using the Process Flow 1, using PEQ, DRC, Clipper, etc.
I2C timing requirements are met.
Here is a scope shot of the output and decoded I2S stream during a pop noise event.
Here is another capture.
Is this a known issue? The rate of occurrence seems t be 1% but often the pops will then continue until power cycle (i.e. configuration happens again) is done.
I have the I2C stream from the configuration from that session if needed.