This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5721: Register settings for PBTL Mode

Part Number: TAS5721
Other Parts Discussed in Thread: CONTROLCONSOLE

I am trying to use the TAS5721 in PBTL mode with two 8 ohm speakers in parallel. 

Attached is the file I am using to set the EVM in PBTL. Could this file be verified if it is correct or missing something? 

Thanks, 
DennisTAS5721_PBTL_AD_LR2_NoEQ_Nov_20_23.CFG