Hello,
We are using the TLV320AIC3110 codec and we have seen that it never appears to go into power down mode i.e. it never writes the value 0x80 to Page 1 Register 46 (0x2E). We only ever see it with value 0x00 or 0x01.
This is our device tree for the codec:
/ { sound0: sound@0 { compatible = "simple-audio-card"; simple-audio-card,name = "MySound"; simple-audio-card,widgets = "Microphone", "Microphone Jack", "Headphone", "Headphone Jack", "Speaker", "Speaker"; simple-audio-card,routing = "MIC1LP", "Microphone Jack", "MIC1RP", "Microphone Jack", "MIC1LP", "MICBIAS", "MIC1RP", "MICBIAS", "Headphone Jack", "HPL", "Headphone Jack", "HPR", "Speaker", "SPL", "Speaker", "SPR"; simple-audio-card,format = "i2s"; simple-audio-card,bitclock-master = <&sound0_master>; simple-audio-card,frame-master = <&sound0_master>; simple-audio-card,bitclock-inversion; simple-audio-card,convert-rate = <48000>; sound0_master: simple-audio-card,cpu { sound-dai = <&i2s1>; system-clock-frequency = <12000000>; }; simple-audio-card,codec { sound-dai = <&codec>; system-clock-frequency = <12000000>; }; }; }; &pinctrl { codec_pins_a: codec_pins_a { pins1 { pinmux = <STM32_PINMUX('H', 2, GPIO)>; /* AUDIO_PWR_EN1 */ }; pins2 { pinmux = <STM32_PINMUX('C', 0, AF6)>, /* CODEC_I2S1_SDO */ <STM32_PINMUX('A', 6, AF5)>, /* CODEC_I2S1_SDI */ <STM32_PINMUX('B', 1, AF5)>, /* CODEC_I2S1_BITCLK / I2S1_CK */ <STM32_PINMUX('B', 0, AF5)>, /* I2S1_MCK */ <STM32_PINMUX('A', 4, AF5)>; /* CODEC_I2S1_WORDCLK / I2S1_WS */ }; }; codec_sleep_pins_a: codec_sleep_pins_a { pins { pinmux = <STM32_PINMUX('H', 2, ANALOG)>, /* AUDIO_PWR_EN1 */ <STM32_PINMUX('C', 0, ANALOG)>, /* CODEC_I2S1_SDO */ <STM32_PINMUX('A', 6, ANALOG)>, /* CODEC_I2S1_SDI */ <STM32_PINMUX('B', 1, ANALOG)>, /* CODEC_I2S1_BITCLK / I2S1_CK */ <STM32_PINMUX('B', 0, ANALOG)>, /* I2S1_MCK */ <STM32_PINMUX('A', 4, ANALOG)>; /* CODEC_I2S1_WORDCLK / I2S1_WS */ }; }; }; &i2s1 { status = "okay"; pinctrl-names = "default", "sleep"; pinctrl-0 = <&codec_pins_a>; pinctrl-1 = <&codec_sleep_pins_a>; /* Sleep pins */ clock-names = "pclk", "i2sclk", "x8k", "x11k"; clocks = <&rcc SPI1>, <&rcc SPI1_K>, <&scmi_clk CK_SCMI_PLL3_Q>, <&scmi_clk CK_SCMI_PLL3_R>; }; &i2c1 { pinctrl-names = "default", "sleep"; pinctrl-0 = <&i2c1_pins_a>; pinctrl-1 = <&i2c1_sleep_pins_a>; i2c-scl-rising-time-ns = <96>; i2c-scl-falling-time-ns = <3>; clock-frequency = <100000>; status = "okay"; /* spare dmas for other usage */ /delete-property/dmas; /delete-property/dma-names; codec: codec@18 { compatible = "ti,tlv320aic3110"; reg = <0x18>; #sound-dai-cells = <0>; status = "okay"; reset-gpios = <&gpiof 6 GPIO_ACTIVE_LOW>; ai31xx-micbias-vg = <MICBIAS_2_0V>; // ai31xx-ocmv = <3>; /* Regulators */ HPVDD-supply = <&scmi_v3v3_sw>; /* 3V3_CODEC */ SPRVDD-supply = <&v5v0_ao>; /* 5V0_CODEC */ SPLVDD-supply = <&v5v0_ao>; /* 5V0_CODEC */ AVDD-supply = <&scmi_v3v3_sw>; /* 3V3_CODEC */ IOVDD-supply = <&scmi_v3v3_sw>; /* 3V3_CODEC */ DVDD-supply = <&scmi_v1v8_periph>; /* 1V8_CODEC */ }; };
Do you know what could be the problem here and what I could do to fix this?
Presumably, the codec should be in Power Down mode until there is a request to play some audio,right?
Thank you.