Dear team,
I am using TLV320AIC3120 AUDIO CODEC.
I'd like to have some information about these below.
1) When using I2S related pins (VDD18) and SDA/SCL (PU VCC_1.8V), does IOVDD also need to supply 1.8V power?
2) Is simultaneous entry into Power SQ DVDD/IODVDD possible?
3) When IOVDD is 1.8V, is the I2S master/slave timing the same as the datasheet contents?
Best regards,