This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5755MEVM: PurePathConsole3 application no response when EVM connect to PC

Part Number: TAS5755MEVM


Hi,

I have a problem when I use PPC3, below is my environment 

OS: Win10

HW: TAS5755MEVM + MC57xxPSIA

My problem is: that the PPC3 app UI will freeze when MC57xxPSIA connects (USB). The UI will work when I remove the device immediately. 

I have done the below check

1. check the device manager when the device connects. A new device appears in “device manager-> Human Interface Device->  USB 輸入裝置”. It looks like the device working fine.

2. I have download and try the “TAS57X1 Graphical Design Environment (GDE)”. It can work without problem, I can use this tool to turn on/off mute. And I can play the audio with this hardware. 

anyoune have suggestion?