Part Number: PCM9211
Other Parts Discussed in Thread: PCM1794
Hello,
I noticed the following strange behavior:
The signal comes in via RXIN6 and is sent to TXOUT and RECOUT1 in parallel:
Register 34: B11000110
Register 36: B00000110
From the MPO0 output the signal goes to a DAC.
If TXOUT is routed to MPO0 (register 78: B00001101), an impulse response of the DAC measured via ADC shows significantly more ringing than if the same signal is routed via RECOUT1 (register 78: B00001111)


At the same time, the measurement of frequency response and THD is absolutely identical. I also recorded a piece of audio as a digital signal at the output of the PCM9211 and did a bit comparison. In both cases, the audio is exactly bit-identical. Thus: No problem is seen in static measurements and with real audio signal. Differences only become apparent with a short pulse (see pictures).
Does anyone have any idea what's happening here?
Furthermore: If I send the signal not as AES3, but as I2S or left justified or right justified signal from the MAIN OUT to the DAC, the result is the same picture as TXOUT: a lot of ringing.
If I remember correctly, the DIR is bypassed via RECOUT. So it looks like something strange is happening in DIR.
By the way, all measurements at 192kHz.
Best wishes
Ralf