Part Number: TLV320AIC3254
Hi ti team,
Can you configure a file of I2S input LOL output to me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
This script comes from the EVM GUI and configures playback to the line outputs. You can use this as a starting point. Please study it and make adjustments according to your set up.
Thanks,
Jeff McPherson
###############################################
# Low Power Stereo Playback
# ---------------------------------------------
# PowerTune mode PTM_P1 is used for low
# power 16-bit audio.
#
# For normal USB Audio, no hardware change
# is required.
#
# If using an external interface, SW2.4 and
# SW2.5 of the USB-ModEVM must be set to
# HI and clocks can be connected to J14 of
# the USB-ModEVM.
#
# Audio is routed to both headphone and
# line outputs.
###############################################
###############################################
# Software Reset
###############################################
#
# Select Page 0
w 30 00 00
#
# Initialize the device through software reset
w 30 01 01
#
###############################################
###############################################
# Clock Settings
# ---------------------------------------------
# The codec receives: MCLK = 11.2896 MHz,
# BLCK = 2.8224 MHz, WCLK = 44.1 kHz
###############################################
#
# Select Page 0
w 30 00 00
#
# NDAC = 1, MDAC = 4
w 30 0b 81 84
#
# DOSR = 64
w 30 0d 00 40
###############################################
###############################################
# Signal Processing Settings
###############################################
#
# Select Page 0
w 30 00 00
#
# Set the DAC Mode to PRB_P8
w 30 3c 08
#
###############################################
###############################################
# Initialize Codec
###############################################
#
# Select Page 1
w 30 00 01
#
# Disable weak AVDD in presence of external
# AVDD supply
w 30 01 08
#
# Enable Master Analog Power Control
w 30 02 00
#
# Set the input powerup time to 3.1ms (for ADC)
# w 30 47 32
#
# Set the REF charging time to 40ms
w 30 7b 01
#
###############################################
##############################################
# Playback Setup
###############################################
#
# Select Page 1
w 30 00 01
#
# De-pop
w 30 14 25
#
# Route LDAC/RDAC to HPL/HPR
w 30 0c 08 08
#
# Route LDAC/RDAC to LOL/LOR
w 30 0e 08 08
#
# Set the DAC PTM mode to PTM_P1
w 30 03 08 08
#
# Power up HPL/HPR and LOL/LOR drivers
w 30 09 3C
#
# Unmute HPL/HPR driver, + 14dB for PTM_P1 compensation
w 30 10 0E 0E
#
# Unmute LOL/LOR driver, + 14dB for PTM_P1 compensation
w 30 12 0E 0E
#
# Select Page 0
w 30 00 00
#
# DAC => 0dB
w 30 41 00 00
#
# Power up LDAC/RDAC
w 30 3f d6
#
# Unmute LDAC/RDAC
w 30 40 00
#
###############################################