Dear team,
I kindly request you to provide alternate suggestions to PCM2704 as this device is NRND. We need the device with USB interface, also with longevity for next 10-12 years. Temperature Range from: -40 to +85/+1105/+125.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
I kindly request you to provide alternate suggestions to PCM2704 as this device is NRND. We need the device with USB interface, also with longevity for next 10-12 years. Temperature Range from: -40 to +85/+1105/+125.
Hi Mayur,
The PCM2704 is still an active device. Can you share where you saw it was NRND?
Thanks,
Jeff McPherson
Dear Jeff,
It is written on top of page 3 of datasheet.

Also the recommended operating temperature is from -25, we need an alternate which works from -40 to +85 or above.
Hi Mayur,
Unfortunately we don't have any USB interfacing DAC/Codecs that have a operating temp range down to -40C
Best regards,
Jeff McPherson