Hello,
We saw in our Project that the Thermal Foldback don't work and the TAS temperature rises all the way to the Thermal Shutdown. We have the Low Latency Path Enabled, is the Thermal Folback one of the function that is disabled by default when the LLP is active?
Anyway on the PurePath Console I can see that there are other settings that can be configured besides the 0xE4 register, but they are not indicated on the datasheet. How can I set the Attack Rate, the Release Rate and the Hold Time using registers? By now I copy what i see in the I2C monitor of the PurePath Controller, but I'm not sure if I am doing it correctly and I was wondering if there is some kind of documentation.
Regards, Marco